Hardware requirements
Micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Short JP52 1-2 and JP50 1-2.
To make i2c example work, connections needed to be as follows: I2C7 connected to I2C2 SCL P1_30(J8-5) –> P1_25(J8-4) SDA P1_21(J8-6) –> P1_24(J8-3)
Prepare the Demo
Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.