Toolchain supported
IAR embedded Workbench 8.22.1
Keil MDK 5.24a
MCUXpresso10.2.0
Hardware requirements
Micro USB cable
LPCXpresso804 board
CapTouch Shield board
Personal Computer
Board settings
Remove JP3, JP21, JP22, JP23, JP25 and C13 on LPCXpresso804 board. Short R6 on CapTouch Shield board
Prepare the Demo
Connect a micro USB cable between the host PC and the CMSIS DAP USB port (CN2) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The CAPT sample data is shown in the terminal, touch the electrode plate to see sample data change.