Hardware requirements
Micro USB cable
LPCXpresso804 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the CMSIS DAP port(CN2 on the board).
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
IAP example
PartID: XXXXX
The major version is: XXXX
The minor version is: XXXX
Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX
End of IAP Example