Functional description
This demo is to show how the various power mode can switch to each other. There is one known issue that terminal may receive mess code after enter deep power down mode, it is caused by the uart TX pin state changed by the MCU under deep power down mode. As the RM says, all the functional pins are tri-stated in deep power down mode except for the WAKEUP pin and the RESET pin. So the state change will be captured by the virtual com port as mess code. Software has no workaround for the issue.
Hardware Requirements
Mini/micro USB cable
LPCXpresso845MAX board
Personal Computer
Board Settings
No special settings are required.
Run the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP port(J4 on the board).
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the
[Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).
Launch the debugger in your IDE to begin running the demo.
Expected Result
Power mode switch Demo for LPC8xx.
Selecct an option
1. Sleep mode
2. Deep Sleep mode
3. Power Down mode
4. Deep power down mode
/* after select power mode, terminal will output */ Select wakeup source
1. Wkt timer
2. SW2, wakeup key
3. SW3, reset key
/* after wakeup, terminal will output */ Wakeup.