Hardware requirements
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 imx93_m33_TCM_power_mode_switch.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0
Append “${mcore_clk}” in u-boot “mmcargs” env, before booting linux. => run prepare_mcore => setenv mmcargs ‘setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot}’
You can also test power_mode_switch function with flash.bin. After flash.bin compilation, please load the bianry by using “UUU” command. For flash.bin test mode, please skip step 4.
Running the demo
Mcore debug console shows the menu to command the MCU to the target power mode. The target power mode can be wakeup by LPTMR and LPUART. SYSTEM SLEEP flow: In linux console use command “echo mem > /sys/power/state” to suspend A55, then select SUSPEND mode in Mcore debug console. The STBY LED on board will light with RED color. NOTE: M33 wakeup A55 by using MU interrupt “GCR[GIR1]”. Please ensure the A55 already in SUSPEND mode, then press “W” button in Mcore debug console. Or you will meet call trace info in linux. NOTE: Please do not perform M33 Root clock switching concurrently with A-core suspend operations! If we change the M-core root clock while the A-core is suspended, the function for M-core to wake up A-core will hang.
The log below shows the output of the power mode switch demo in the terminal window:
Start SRTM communication
Task 1 is working now
#################### Power Mode Switch Task ####################
Build Time: Feb 3 2023--21:35:13
Core Clock: 200000000Hz
Select the desired operation
Press A to enter: Normal RUN mode
Press B to enter: WAIT mode
Press C to enter: STOP mode
Press D to enter: SUSPEND mode
Press W to wakeup A55 core
Waiting for power mode select..