Hardware requirements
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
The example requires doing connection between LPSPI3(as master) pins and FLEXIO1(as slave) pins.
IOMUXC_PAD_GPIO_IO09__LPSPI3_SIN(J16-21), FLEXIO_SPI_SOUT_PIN(J16-3) connected
IOMUXC_PAD_GPIO_IO10__LPSPI3_SOUT(J16-19), FLEXIO_SPI_SIN_PIN(J16-5) connected
IOMUXC_PAD_GPIO_IO11__LPSPI3_SCK(J16-23), FLEXIO_SPI_CLK_PIN(J16-7) connected
IOMUXC_PAD_GPIO_IO08__LPSPI3_PCS0(J16-24), FLEXIO_SPI_PCS_PIN(J16-29) connected
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPSPI Master interrupt - FLEXIO SPI Slave interrupt example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is FLEXIO SPI slave call back.
LPSPI master <-> FLEXIO SPI slave transfer all data matched!
End of Example.