Hardware requirements

  • USB Type-C cable

  • Network cable RJ45 standard

  • MCIMX93AUTO-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J601) as default.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.