Hardware requirements
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
The example requires connecting the FLEXIO1 pins with the USB2COM pins The connection should be set as follows:
FLEXIO_RX(J1001-5) on base board, TX of USB2COM connected
FLEXIO_TX(J1001-3) on base board, RX of USB2COM connected
GND(J1005-7) on base board, Ground of USB2COM connected
Please note this application can’t support running with Linux BSP!
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict. Tips: After you insert the USB2COM, a new USBCOM will be found. The function output in new USBCOM.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
FLEXIO UART RX ring buffer example
Send back received data
Echo every 8 bytes