Hardware requirements
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Build the project and generate the flash.bin file of single boot or low power boot. Refer to the ‘Getting Started with MCUXpresso SDK for MCIMX93-EVK.pdf’.
Connect a type-c USB cable between the host PC and the J1401 USB port on the target board.
Connect 12~20V power supply to the board.
Download flash.bin into sd/emmc/flash with uuu. Refer to ‘Getting Started with MCUXpresso SDK for MCIMX93-EVK.pdf’
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Switch the SW301 to re-power the board.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
High Byte test success
----- Refresh test start -----
----- None-window mode -----
Refresh wdog32 0 time
Refresh wdog32 1 time
Refresh wdog32 2 time
Refresh wdog32 3 time
Refresh wdog32 4 time
Refresh wdog32 5 time
Refresh wdog32 6 time
Refresh wdog32 7 time
Refresh wdog32 8 time
Refresh wdog32 9 time
----- Window mode -----
Refresh wdog32 0 time
Refresh wdog32 1 time
Refresh wdog32 2 time
----- Refresh test success  -----
----- End of WDOG32 example  -----