Hardware requirements
USB Type-C cable
MCIMX93-QSB board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No need special setting.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /sdk20-app.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
USART EDMA example
Send back received data
Echo every 8 characters