Hardware requirements
USB Type-C cable
MCIMX93-QSB board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Oscilloscope
Board settings
CM33: connect J1406-3 and J1406-7(GND) to Oscilloscope
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1708 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM example for output compare
You will see the output signal toggle
Probe the signal using an oscilloscope