Hardware requirements
Micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TSI_V6 Self-Cap mode Example Start!
Calibrated counters for channel 0 is: 4328
Calibrated counters for channel 1 is: 4310
Calibrated counters for channel 2 is: 5095
Calibrated counters for channel 3 is: 65535
Calibrated counters for channel 4 is: 8748
Calibrated counters for channel 5 is: 8512
Calibrated counters for channel 6 is: 7375
Calibrated counters for channel 7 is: 7464
Calibrated counters for channel 8 is: 4935
Calibrated counters for channel 9 is: 4872
Calibrated counters for channel 10 is: 65535
Calibrated counters for channel 11 is: 5266
Calibrated counters for channel 12 is: 5419
Calibrated counters for channel 13 is: 4494
Calibrated counters for channel 14 is: 4822
Calibrated counters for channel 15 is: 4932
Calibrated counters for channel 16 is: 5070
Calibrated counters for channel 17 is: 65535
Calibrated counters for channel 18 is: 65535
Calibrated counters for channel 19 is: 4056
Calibrated counters for channel 20 is: 8420
Calibrated counters for channel 21 is: 4048
Calibrated counters for channel 22 is: 65535
Calibrated counters for channel 23 is: 65535
Calibrated counters for channel 24 is: 65535
NOW, comes to the software trigger scan using polling method!
Channel 19 Normal mode counter is: 4056
NOW, comes to the software trigger scan using interrupt method!
Channel 19 Normal mode counter is: 4183
NOW, comes to the hardware trigger scan method!
After running, touch pad E1 each time, you will see LED toggles.