Hardware requirements
Mini/micro USB cable
RJ45 Network cable
MCX-N5XX-EVK board
Personal Computer
Board settings
Connect JP13 2-3 pin. Populate R274 to sync reference clock. Note that when HW flash swapping feature is used the images are swapped so that address range of the primary image translates to the range of the secondary image and vice versa. The web page of the ota_mcuboot_server example shows image state as read from the bus so when HW flash swapping is used it will not match with the physical image state - the slots will be swapped.