Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
DAC output pin: J1-4(P4_2)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
A multimeter may be used to measure the DAC output voltage (Connector J1-4).
Running the demo
When the demo runs successfully, the log would be seen on the debug console terminal like:
DAC buffer interrupt Example. Press any key to trigger the DAC… DAC next output: 200 DAC next output: 300 DAC next output: 400 DAC next output: 500 DAC next output: 600 DAC next output: 700 DAC next output: 800 DAC next output: 900
Then user can measure the DAC output pin to check responding voltage.