Hardware requirements

  • Mini/micro USB cable

  • MCX-N9xx-EVK board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Jumper setting:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 - 8           SIN         J2 - 10
SIN        J2 - 10          SOUT        J2 - 8
SCK        J2 - 12          SCK         J2 - 12
PCS0       J2 - 6           PCS0        J2 - 6
GND        J2 - 14          GND         J2 - 14

Other jumpers keep default configuration.

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.