Hardware requirements
Micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the host PC and the MCU-Link USB port (J5) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
PINT Pin interrupt example
PINT Pin Interrupt events are configured
Press corresponding switches to generate events
This example configures “Pin Interrupt 0” to be invoked when SW3 switch is pressed by the user. The interrupt callback prints “PINT Pin Interrupt 0 event detected”. “Pin Interrupt 1” is is configured to be invoked when SW2 is pressed. The interrupt callback prints “PINT Pin Interrupt 1 event detected”.