Hardware requirements
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
Example output:
GPIO Driver example
The LED is taking turns to shine.
Standard port read: 1c100c
Masked port read: 1c0000
Port state: 18100c
Port state: 10100c
Port state: 18100c
Port state: 10100c
...
When press sw4 the LED BLUE will toggle.