Hardware requirements
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings
Output signal Board location
SCT0_OUT4(PIO0_7) J20-5
SCT0_OUT5(PIO0_6) J20-6
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output in the terminal window:
SCTimer example to use it in 16-bit mode
The example shows both 16-bit counters running and toggling an output periodically
Probe an oscilloscope to the output pins described in board settings, you will see one output signal toggling at 5Hz and another output signal toggling at 2.5Hz.