Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(SPI1) connect to SLAVE(SPI1)
Pin Name Board Location Pin Name Board Location
SOUT J2 pin 13 SIN J2 pin 11
SIN J2 pin 11 SOUT J2 pin 13
SCK J2 pin 9 SCK J2 pin 9
PCS0 J2 pin 15 PCS0 J2 pin 15
Other jumpers keep default configuration.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.