Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
USB to Serial Converter
Personal Computer
Board settings
The connection should be set as following:
J1-1(PTA16), TX of USB2COM connected
J1-3(PTA17), RX of USB2COM connected
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for USB2COM serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the USB2COM terminal like:
Lpuart polling example with seven data bits
Board will send back received characters