Hardware requirements

  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(LPSPI0)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 7                         SOUT        J2 pin 13
SIN        J1 pin 13                        SIN         J2 pin 11
SCK        J1 pin 15                        SCK         J2 pin 9
PCS0       J1 pin 5                         PCS0        J2 pin 15

Prepare the Demo

  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FLEXIO Master - LPSPI Slave interrupt example start.
This example use one flexio spi as master and one lpspi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXIO_SPI_master -- LPSPI_slave   
       CLK        --    CLK  
       PCS        --    PCS  
       SOUT       --    SIN  
       SIN        --    SOUT 
This is LPSPI slave call back.
FLEXIO SPI master <-> LPSPI slave transfer all data matched!

End of example.