Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
MASTER(LPSPI0) connect to SLAVE(FlexIO SPI)
Pin Name Board Location Pin Name Board Location
SOUT J2 pin 13 SOUT J1 pin 7
SIN J2 pin 11 SIN J1 pin 13
SCK J2 pin 9 SCK J1 pin 15
PCS0 J2 pin 15 PCS0 J1 pin 5
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
LPSPI Master interrupt - FLEXIO SPI Slave interrupt example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is FLEXIO SPI slave call back.
LPSPI master <-> FLEXIO SPI slave transfer all data matched!
End of Example.