Hardware requirements

  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

NOTE: Depending on the toolchain configuration, the benchmark result might be different.

CMSIS DSP benchmark vector test start.
PQ_VectorLnF32Test: xxx
PQ_VectorLnQ31Test: xxx
PQ_VectorInvF32Test: xxx
PQ_VectorInvQ31Test:  xxx
PQ_VectorSqrtF32Test: xxx
PQ_VectorSqrtQ31Test: xxx
PQ_VectorInvSqrtF32Test: xxx
PQ_VectorInvSqrtQ31Test: xxx
PQ_VectorEtoxF32Test: xxx
PQ_VectorEtoxQ31Test: xxx
PQ_VectorEtonxF32Test: xxx
PQ_VectorEtonxQ31Test: xxx
PQ_BiquadCascadedf2F32Test: xxx
PQ_BiquadCascadedf2Q31Test: xxx
PQ_VectorLnFPTest: xxx
PQ_VectorLnFXTest: xxx
PQ_VectorInvFPTest: xxx
PQ_VectorInvFXTest: xxx
PQ_VectorSqrtFPTest: xxx
PQ_VectorSqrtFXTest: xxx
PQ_VectorInvSqrtFPTest: xxx
PQ_VectorInvSqrtFXTest: xxx
PQ_VectorEtoxFPTest: xxx
PQ_VectorEtoxFXTest: xxx
PQ_VectorEtonxFPTest: xxx
PQ_VectorEtonxFXTest: xxx
PQ_16ByteBiquadCascadedf2FPTest: xxx
PQ_16ByteBiquadCascadedf2FXTest: xxx
PQ_VectorSqrtQ31Test: xxx
PQ_VectorSqrtQ15Test: xxx
PQ_VectorSinF32Test: xxx
PQ_VectorSinQ31Test: xxx
PQ_VectorSinQ15Test: xxx
PQ_VectorCosF32Test: xxx
PQ_VectorCosQ31Test: xxx
PQ_VectorCosQ15Test: xxx

CMSIS DSP benchmark vector test succeeded.