Hardware requirements

  • Micro USB cable

  • Target board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-LINK USB port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

PMC Temperature Sensor Demo
ADC Full Range: 65536
Please press any key to get temperature from the internal temperature sensor.
Current temperature: 28.59
Current temperature: 28.67