Hardware requirements
Mini/micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
MASTER(FlexIO SPI) connect to SLAVE(FlexIO SPI)
Pin Name Board Location Pin Name Board Location
MOSI J5 Pin 6 MOSI J5 pin 6
MISO J5 pin 3 MISO J5 Pin 3
SCK J5 pin 4 SCK J5 pin 4
PCS J5 pin 5 PCS J5 pin 5
GND J6 pin 7 GND J6 pin 7
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FlexIO SPI edma example
Master Start...
Master runs successfully!