Hardware requirements
Micro USB cable
mimxrt700evk
Personal Computer
One of the following modules:
Embedded Artists 1XK M.2 Module (EAR00385) - direct M2 connection.
Embedded Artists 1ZM M.2 Module (EAR00364) - direct M2 connection.
Embedded Artists 2EL M.2 Module (Rev-A1) - direct M2 connection.
Embedded Artists 2LL M.2 Module (EAR00500) - direct M2 connection.
Board settings
Before building the example application select Wi-Fi module macro in the app_bluetooth_config.h. (see #define WIFI_
Jumper settings for RT700-EVKC (enables external 5V supply):
remove J2 5-6 connect J2 1-2 connect J45 with external power(controlled by SW4)
Murata Solution Board settings
Embedded Artists 1XK module datasheet: https://www.embeddedartists.com/doc/ds/1XK_M2_Datasheet.pdf Embedded Artists 1ZM module datasheet: https://www.embeddedartists.com/doc/ds/1ZM_M2_Datasheet.pdf Embedded Artists 2EL module datasheet: https://www.embeddedartists.com/doc/ds/2EL_M2_Datasheet.pdf Embedded Artists 2LL module datasheet: https://www.embeddedartists.com/wp-content/uploads/2024/12/2LL_M2_Datasheet.pdf
Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW7 or power off and on the board to run the application.