Hardware requirements

  • Micro USB cable

  • RD-RW61X-BGA board

  • Personal Computer

  • headphones with 3.5 mm stereo jack

Board settings

Connect JP50, JP51; Disconnect JP9, JP11

Prepare the Demo

  1. Connect headphones to Audio HP connector (J4).

  2. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo

Headphones will play a sine wave sound. The log below shows example output of the I2S driver demo in the terminal window:

Configure codec
Configure I2S
Setup looping playback of sine wave