Hardware requirements

  • Micro USB cable

  • RD-RW61X-BGA board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the terminal will display similar information like the following:

ELS hash example

============================ SHA224 one shot:pass SHA256 one shot:pass SHA256 streaming example:pass SHA256 long message example:pass SHA384 one shot:pass SHA512 one shot:pass

============================ RESULT: All 6 test PASS!! ELS example END