Hardware requirements

  • Micro USB cable

  • RD-RW61X-BGA board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the terminal will display similar information like the following:

ELS PKC asymmetric cipher example

============================ PKC ECC keygen sign verify:pass PKC RSA no-verify:pass PKC RSA sign no-encode:pass PKC RSA-PSS sign SHA256:pass PKC RSA-PSS verify SHA256:pass PKC ECC Curve25519:pass TLS Master session keys:pass

============================ RESULT: All 7 test PASS!! ELS example END