Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J14-1
TX of USB2COM to J16-1
GND of USB2COM to J25-10
Prepare the Demo
Connect USB to Com Converter between the host PC and the port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the example runs successfully, the log would be seen on the UART Terminal port which connected to the USB2COM like:
LPUART DMA ring buffer example.
Board will send back received characters: