Maestro record example

Table of content

Overview

The Maestro record example demonstrates audio processing on the ARM cortex core utilizing the Maestro Audio Framework library.

The application is controlled by commands from a shell interface using serial console.

Depending on target platform or development board there are different modes and features of the demo supported.

  • Loopback - The application demonstrates a loopback from the microphone to the speaker without any audio processing. Mono, stereo or multichannel mode can be used, depending on the hardware, see table below.

  • File recording - The application takes audio samples from the microphone inputs and stores them to an SD card as an PCM file. The PCM file has following parameters:

    • Mono and stereo : 2 channels, 16kHz, 16bit width

    • Multi-channel (AUD-EXP-42448): 6 channels, 16kHz, 32bit width

  • Voice control - The application takes audio samples from the microphone input and uses the VIT library to recognize wake words and voice commands. If a wake word or a voice command is recognized, the application write it to the serial terminal.

  • Encoding - The application takes PCM samples from memory and sends them to the Opus encoder. The encoded data is stored in memory and compared to a reference. The result of the comparison is finally written into the serial terminal.

As shown in the table below, the application is supported on several development boards, and each development board may have certain limitations, some development boards may also require hardware modifications or allow to use of an audio expansion board. Therefore, please check the supported features and Hardware modifications or Example configuration sections before running the demo.

Mode Loopback File recording Voice control Encoding
Feature Audio input / output [num of channels] Audio inputs [num of channels] Audio inputs [num of channels] Additional libraries Encoder
On board codec DMICs aud-exp-42448 On board codec DMICs aud-exp-42448 On board codec DMICs aud-exp-42448 VIT VoiceSeeker OPUS
EVKC-MIMXRT1060 1 / 1 X 1-6 / 1-6 1 X 1-6 1 X 1-2 OK OK OK
EVKB-MIMXRT1170 0 / 1-2 1-2 X X 1-2 X X 1-2 X OK OK OK
LPCXpresso55s69 1-2 / 1-2 X X 1-2 / 1-2 X X 1 X X OK X X
EVK-MCXN5XX 1-2 / 1-2 1-2 X 1-2 X X 1-2 X X OK X OK
RW612BGA 0 / 1-2 1-2 X X X X X 1-2 X OK OK X
- Dark green - Fully supported and enabled by default.
- Orange - Supported with some limitations and enabled by default. See the limitations section below.
- Light green - Supported, but only available after some SW or HW modification. More information about modification can be found in the [Example configuration](#example-configuration) section.
- X - Not supported.

Limitations:

  • Note:

    • LPCXPresso55s69 - MCUXpresso IDE project default debug console is semihost

  • Addition labraries

    • VIT:

      • The VIT is supported only in the MCUXpresso IDE and ARMGCC.

      • LPCXpresso55s69 - The VIT is disabled by default due to insufficient memory. To enable it, see the Example configuration section.

      • EVK-MCXN5XX - Some VIT models can’t fit into memory. In order to free some space it is necessary to disable SD card handling and opus encoder. To disable it, see the Example configuration section.

    • VoiceSeeker:

      • The VoiceSeeker is supported only in the MCUXpresso IDE and ARMGCC.

  • Encoder

    • OPUS:

      • LPCXpresso55s69 - The encoder is not supported due to insufficient memory.

  • The File recording mode is not supported on RW612BGA development board due to missing SD card slot.

Known issues:

  • EVKB-MIMXRT1170 - After several tens of runs (the number of runs is not deterministic), the development board restarts because a power-up sequence is detected on the RESET pin (due to a voltage drop).

More information about supported features can be found on the Supported features page.

Hardware requirements

  • Desired development board

  • Micro USB cable

  • Headphones with 3.5 mm stereo jack

  • Personal computer

  • Optional:

  • LPCXpresso55s69:

    • Source of sound with 3.5 mm stereo jack connector

Hardware modifications

Some development boards need some hardware modifications to run the application. If the development board is not listed here, its default setting is required.

  • EVKB-MIMXRT1170:

    1. Please remove below resistors if on board wifi chip is not DNP:

      • R228, R229, R232, R234

    2. Please make sure R136 is weld for GPIO card detect.

  • EVK-MCXN5XX:

    • Short: JP7 2-3, JP8 2-3, JP10 2-3, JP11 2-3

  • RW612BGA:

    • Connect: JP50; Disconnect JP9, JP11

Preparation

  1. Connect a micro USB cable between the PC host and the debug USB port on the development board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Insert the headphones into the Line-Out connector (headphone jack) on the development board.

  5. LPCXpresso55s69:

    • Insert source of sound to audio Line-In connector (headphone jack) on the development board.

  6. Either press the reset button on your development board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you should see similar output on the serial terminal as below:

    *******************************
    Maestro audio record demo start
    *******************************

    Copyright  2022  NXP
    [APP_SDCARD_Task] start
    [APP_Shell_Task] start

    >> [APP_SDCARD_Task] SD card drive mounted

Type help to see the command list. Similar description will be displayed on serial console:

    >> help

    "help": List all the registered commands

    "exit": Exit program

    "version": Display component versions

    "record_mic": Record MIC audio and perform one (or more) of following actions:
    - playback on codec
    - perform VoiceSeeker processing
    - perform voice recognition (VIT)
    - store samples to a file.

    USAGE: record_mic [audio|file|<file_name>|vit] 20 [<language>]
    The number defines length of recording in seconds.

    Please see the project defined symbols for the languages supported.
    Then specify one of: en/cn/de/es/fr/it/ja/ko/pt/tr as the language parameter.
    For voice recognition say supported WakeWord and in 3s frame supported command.
    Please note that this VIT demo is near-field and uses 1 on-board microphone.

    NOTES: This command returns to shell after the recording is finished.
           To store samples to a file, the "file" option can be used to create a file
           with a predefined name, or any file name (without whitespaces) can be specified
           instead of the "file" option.

    "opus_encode": Initializes the streamer with the Opus memory-to-memory pipeline and
    encodes a hardcoded buffer.

Details of commands can be found here.

Example configuration

The example can be configured by user. There are several options how to configure the example settings, depending on the environment. For configuration using west and Kconfig, please follow the instructions here. Before configuration, please check the table to see if the feature is supported on the development board.

  • Connect AUD-EXP-42448:

    • EVKC-MIMXRT1060:

      1. Disconnect the power supply for safety reasons.

      2. Insert AUD-EXP-42448 into J19 to be able to use the CS42448 codec for multichannel output.

      3. Uninstall J99.

      4. Set the DEMO_CODEC_WM8962 macro to 0 in the app_definitions.h file

      5. Set the DEMO_CODEC_CS42448 macro to 1 in the app_definitions.h file.

      6. Enable VoiceSeeker, see point bellow.

    • Note:

      • The audio stream is as follows:

        • Stereo INPUT 1 (J12) -> LINE 1&2 OUTPUT (J6)

        • Stereo INPUT 2 (J15) -> LINE 3&4 OUTPUT (J7)

        • MIC1 & MIC2 (P1, P2) -> LINE 5&6 OUTPUT (J8)

        • Insert the headphones into the different line outputs to hear the inputs.

        • To use the Stereo INPUT 1, 2, connect an audio source LINE IN jack.

  • Enable VoiceSeeker:

    • On some development boards the VoiceSeeker is enabled by default, see the table above.

    • If more than one channel is used and VIT is enabled, the VoiceSeeker that combines multiple channels into one must be used, as VIT can only work with mono signal.

    • Using MCUXPresso IDE:

      • It is necessary to add VOICE_SEEKER_PROC symbol to preprocessor defines on project level:

        • (Project -> Properties -> C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor)

    • Using Kconfig:

      • Enable the VoiceSeeker in the guiconfig using MCUX_PRJSEG_middleware.audio_voice.components.voice_seeker

  • Enable VIT:

    • LPCXpresso55s69 and MCX-N5XX:

      • In MCUXPresso IDE (SDK package):

        1. Remove SD_ENABLED and STREAMER_ENABLE_FILE_SINK symbols from preprocessor defines on project level.

        2. Add VIT_PROC symbol to preprocessor defines on project level:

          • (Project -> Properties -> C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor)

      • In armgcc in SDK package:

        1. Remove SD_ENABLED and STREAMER_ENABLE_FILE_SINK symbols from preprocessor defines in flags.cmake file.

        2. Remove OPUS_ENCODE=1 and STREAMER_ENABLE_ENCODER preprocessor defines in flags.cmake file.

        3. Add VIT_PROC symbol to preprocessor defines in flags.cmake file.

        4. Remove sdmmc_config.c,.h files from CMakeLists.txt file.

      • In Kconfig:

        1. Disable File sink MCUX_COMPONENT_middleware.audio_voice.maestro.element.file_sink.enable

        2. Make sure SD card support is disabled MCUX_COMPONENT_middleware.sdmmc.sd and MCUX_COMPONENT_middleware.sdmmc.host.usdhc

        3. Make sure sdmmc_config files (.c, .h) is excluded from project build

          • remove mcux_add_source function that adds the sources in reconfig.cmake in maestro_record/cm33_core0 folder

        4. Disable fatfs MCUX_COMPONENT_middleware.fatfs and MCUX_COMPONENT_middleware.fatfs.sd

        5. Disable file utils MCUX_COMPONENT_middleware.audio_voice.maestro.file_utils.enable

        6. Make sure Opus encoder is disabled MCUX_COMPONENT_middleware.audio_voice.maestro.element.encoder.opus.enable

        7. Make sure VIT_PROC symbol is defined

          • remove mcux_remove_macro function that removes the VIT_PROC preprocessor definition in reconfig.cmake in maestro_record folder

        8. Make sure VIT processing is enabled MCUX_PRJSEG_middleware.audio_voice.components.vit

  • VIT model generation:

    • For custom VIT model generation (defining own wake words and voice commands) please use https://vit.nxp.com/

  • Disable SD card handling:

    • In MCUXPresso IDE:

      • Remove SD_ENABLED and STREAMER_ENABLE_FILE_SINK symbols from preprocessor defines on project level:

        • (Project -> Properties -> C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor)

    • In armgcc in SDK package:

      • Remove SD_ENABLED and STREAMER_ENABLE_FILE_SINK symbols from preprocessor defines in flags.cmake file.

    • In Kconfig:

      1. Disable File sink MCUX_COMPONENT_middleware.audio_voice.maestro.element.file_sink.enable

      2. Make sure SD card support is disabled MCUX_COMPONENT_middleware.sdmmc.sd

Functionality

The record_mic or opus_encode command calls the STREAMER_mic_Create or STREAMER_opusmem2mem_Create function from the app_streamer.c file depending on the selected mode.

  • When the Loopback mode is selected, the command calls the STREAMER_mic_Create function that creates a pipeline with the following elements:

    • ELEMENT_MICROPHONE_INDEX

    • ELEMENT_SPEAKER_INDEX

  • When the File recording mode is selected, the command calls the STREAMER_mic_Create function that creates a pipeline with the following elements: - ELEMENT_MICROPHONE_INDEX - ELEMENT_FILE_SINK_INDEX

  • When the Voice control mode is selected, the command calls the STREAMER_mic_Create function that creates a pipeline with the following elements: - ELEMENT_MICROPHONE_INDEX - ELEMENT_VOICESEEKER_INDEX (If VOICE_SEEKER_PROC is defined) - ELEMENT_VIT_INDEX

  • When the Encoding mode is selected, the command calls the STREAMER_opusmem2mem_Create function that creates a pipeline with the following elements: - ELEMENT_MEM_SRC_INDEX - ELEMENT_ENCODER_INDEX - ELEMENT_MEM_SINK_INDEX

Recording itself can be started with the STREAMER_Start function.

Each of the elements has several properties that can be accessed using the streamer_get_property or streamer_set_property function. These properties allow a user to change the values of the appropriate elements. The list of properties can be found in streamer_element_properties.h. See the example of setting property value in the following piece of code from the app_streamer.c file:

    ELEMENT_PROPERTY_T prop;

    prop.prop = PROP_MICROPHONE_SET_NUM_CHANNELS;
    prop.val  = DEMO_MIC_CHANNEL_NUM;
    streamer_set_property(handle->streamer, 0, prop, true);

    prop.prop = PROP_MICROPHONE_SET_BITS_PER_SAMPLE;
    prop.val  = DEMO_AUDIO_BIT_WIDTH;
    streamer_set_property(handle->streamer, 0, prop, true);

    prop.prop = PROP_MICROPHONE_SET_FRAME_MS;
    prop.val  = DEMO_MIC_FRAME_SIZE;
    streamer_set_property(handle->streamer, 0, prop, true);

    prop.prop = PROP_MICROPHONE_SET_SAMPLE_RATE;
    prop.val  = DEMO_AUDIO_SAMPLE_RATE;
    streamer_set_property(handle->streamer, 0, prop, true);

Some of the predefined values can be found in the streamer_api.h.

States

The application can be in 2 different states:

  • Idle

  • Running

Commands in detail

Legend for diagrams:

flowchart TD classDef function fill:#69CA00 classDef condition fill:#0EAFE0 classDef state fill:#F9B500 classDef error fill:#F54D4D A((State)):::state B{Condition}:::condition C[Error message]:::error D[Process function]:::function

help, version

flowchart TD classDef function fill:#69CA00 classDef condition fill:#0EAFE0 classDef state fill:#F9B500 classDef error fill:#F54D4D A((Idle)):::state --> C[Write help or version]:::function B((Running)):::state --> C C --> E((No state change)):::state

record_mic audio <time>

flowchart TD classDef function fill:#69CA00 classDef condition fill:#0EAFE0 classDef state fill:#F9B500 classDef error fill:#F54D4D B((Idle)):::state --> D{time > 0 ?}:::condition D -- Yes --> F[recording]:::function D -- No --> E[Error: Record length must be greater than 0]:::error E --> B F --> C((Running)):::state C -->G{time expired?}:::condition G -- No --> C G -- Yes --> B

record_mic file <time>/record_mic <file_name> <time>

flowchart TD classDef function fill:#69CA00 classDef condition fill:#0EAFE0 classDef state fill:#F9B500 classDef error fill:#F54D4D B((Idle)):::state --> C{time > 0 ?}:::condition C -- Yes --> D{SD card inserted?}:::condition C -- No --> E[Error: Record length must be greater than 0]:::error E --> B D -- Yes --> G{Custom file name?}:::condition G -- Yes --> H[Create custom file name]:::function G -- No --> I[Create default file name]:::function H --> J[Recording]:::function I --> J J --> K((Running)):::state K -->L{time expired?}:::condition L -- No --> K L -- Yes --> B D -- No --> F[Error: Insert SD card first]:::error F --> B

record_mic vit <time> <language>

flowchart TD classDef function fill:#69CA00 classDef condition fill:#0EAFE0 classDef state fill:#F9B500 classDef error fill:#F54D4D B((Idle)):::state --> C{time > 0 ?}:::condition C -- Yes --> E{Selected language?}:::condition C -- No --> D[Error: Record length must be greater than 0]:::error D --> B E -- Yes --> G{Supported language?}:::condition E -- No --> F[Error: Language not selected]:::error F -->B G -- Yes -->I[Recording with voice recognition]:::function G -- No -->H[Error: Language not supported]:::error H --> B I --> J((Running)):::state J -->K{time expired?}:::condition K -- No --> J K -- Yes --> B

opus_encode

flowchart TD classDef function fill:#69CA00 classDef condition fill:#0EAFE0 classDef state fill:#F9B500 classDef error fill:#F54D4D B((Idle)):::state -->C[Encode file]:::function C -->D[Check result]:::function D -->B

Processing Time

Typical execution times of the streamer pipeline for the EVKC-MIMXRT1060 development board are detailed in the following table. The duration spent on output buffers and reading from the microphone is excluded from traversal measurements. Three measured pipelines were considered. The first involves a loopback from microphone to speaker, supporting both mono and stereo configurations. The second pipeline is a mono voice control setup, comprising microphone and VIT blocks. The final pipeline is a stereo voice control setup, integrating microphone, voice seeker, and VIT blocks.

For further details of execution times on individual elements, please refer to the Processing Time document.

streamer

microphone -> speaker 1 channel

40 μs

microphone -> speaker 2 channels

115 μs

microphone -> VIT

7.4 ms

microphone -> voice seeker -> VIT

9.9 ms