Common steps
Download SDK_2.13.0_EVK-MIMXRT1060 and SDK_2.13.0_EVK-MIMXRT1064.
Copy the following folders from RT1060EVK package to RT1064 package:
<install_dir>/components/internal_flash/ <install_dir>/middleware/edgefast_bluetooth/ <install_dir>/middleware/wireless/
.Create a folder named
edgefast_bluetooth_examples/
under<rt1064_install_dir>/boards/evkmimxrt1064/
.Copy the entire folder from
<rt1060evk_install_dir>/boards/evkmimxrt1060/edgefast_bluetooth_examples/peripheral_ht/
to< rt1064_install_dir>/boards/evkmimxrt1064/edgefast_bluetooth_examples/
.Copy clock_config.[c/h] and board.c from
<rt1064_install_dir>/boards/evkmimxrt1064/demo_apps/hello_world/
to<rt1064_installed>/boards/evkmimxrt1064/edgefast_bluetooth_examples/peripheral_ht/
to replace the previous files.Add
#define EDGEFAST_BT_LITTLEFS_MFLASH 1
in<rt1064_install_dir>/boards/ evkmimxrt1064/edgefast_bluetooth_examples/peripheral_ht /app_config.c
.Make the following changes in
<rt1064_installed>/boards/evkmimxrt1064/edgefast_bluetooth/peripheral_ht/board.h
.
Parent topic:Migrate examples from RT1060EVK to RT1064