System requirements
System requirements are based on the requirements for the development tools and the MfgTool application. The recommended PC configuration is 2 GHz processor, 2 GB RAM, and 2 GB free disk space.
Windows OS applications like MfgTool require installation of Visual C++ redistributable 2013 or greater.
To make the MfgTool work, the device needs to be connected to a PC via a USB hub. Sometimes, an extra USB hub is required if all the USB ports on the PC are USB root hub ports.