Features

For downloading an application, the Flashloader supports the following communication interfaces:

  • USB-HID (USB1)

  • LPUART1

It also supports configuring and programming the external flash device in a user-friendly manner. For further details, refer to MCU Flashloader Reference Manual.