Porting examples
Copy a new platform example
The platform USB examples directory is shown in the following figure.
|
|
Copy the existed example’s whole directory from the similar platform, which ensures that all example source files and project files are copied.
For example, copy the twrk22f120m/usb/usb_device_audio_generator_lite to the twrkxx/usb location, which ensures that sources files and project files for usb_device_audio_generator_lite example are copied.
Parent topic:Porting examples
Porting the example
For different examples, different pins are used. As a result, the pin_mux.c/h files are needed to assign different pins to a specific functionality. Check the board schematic for correct pin settings.
Example-related port pin configurations are required in the following files:
|
|
Ensure the BOARD_InitPins
function is implemented in the pin_mux.c file. In this function, the port clock and pin mux are initialized. Ensure that the BOARD_InitHardware
calls the function. The BOARD_InitHardware
function will be introduced later.
For example, on the TWR-K65F180M board, the VBUS of the USB Host is controlled by the PORTD_8 as a GPIO. Therefore, the PORTD clock needs to be enabled first and then the PORTD_8 configured to GPIO functionality. The debug console uses UART2. The TX/RX pins are PORTE_16 and PORTE_17. As a result, the clock of PORTE needs to be enabled first and then the PORTE_16 and PORTE_17 configured to alternative 3.
This is example code for TWR-K65F180M:
void BOARD_InitPins(void)
{
/* Initialize UART2 pins below */
CLOCK_EnableClock(kCLOCK_PortE);
PORT_SetPinMux(PORTE, 16u, kPORT_MuxAlt3);
PORT_SetPinMux(PORTE, 17u, kPORT_MuxAlt3);
/* Initialize usb vbus pin */
CLOCK_EnableClock(kCLOCK_PortD);
PORT_SetPinMux(PORTD, 8u, kPORT_MuxAsGpio);
}
Check the specific board design to find out which port is used to control the USB VBUS and which port is used for the debug console. For example, in the customer’s board design, the PORTC_15 is used to control the USB VBUS, and PORTD_1 and PORTD_2 is used for debug console. The following shows the example code:
void BOARD_InitPins(void)
{
/* Initialize UART2 pins below */
CLOCK_EnableClock(**kCLOCK\_PortD**);
PORT_SetPinMux(**PORTD, 1u,** kPORT_MuxAlt3);
PORT_SetPinMux(**PORTD, 2u,** kPORT_MuxAlt3);
/* Initialize usb vbus pin */
CLOCK_EnableClock(**kCLOCK\_PortC**);
PORT_SetPinMux(**PORTC, 15u,** kPORT_MuxAsGpio);
}
The VBUS must output high. The following is example code for TWR-K65F180M:
void BOARD_InitHardware(void)
{
gpio_pin_config_t pinConfig;
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
/* vbus gpio output high */
pinConfig.pinDirection = kGPIO_DigitalOutput;
pinConfig.outputLogic = 1U;
GPIO_PinInit(PTD, 8U, &pinConfig);
}
The user can change the function as follows:
void BOARD_InitHardware(void)
{
gpio_pin_config_t pinConfig;
BOARD_InitPins();
**BOARD\_BootClockxxx**();
BOARD_InitDebugConsole();
/* vbus gpio output high */
pinConfig.pinDirection = kGPIO_DigitalOutput;
pinConfig.outputLogic = 1U;
GPIO_PinInit(PTC, 15U, &pinConfig);
}
Parent topic:Porting examples
Modify the example project
USB example project files are kept in the example directory, as shown in the following figure.
|
|
Open the project and change the SoC.
Note:
Check the project SoC and update to the porting platform SoC.
Update the SoC full name, platform name, and board type name macros if the SoC is updated. For example, for TWR-K22F120M, update the CPU_MK22FN512VDC12, TWR_K22F120M, and TOWER macros.
Check the files in startup group, for example (IAR):
|
|
Ensure that the system\_MK22F51212.c, system\_MK22F51212.h, and strtup\_MK22F51212.s are the porting SoC files. Also change the include path.
Check the files in the platform/clock group, for example (IAR):
|
|
Ensure that the fsl\_clock\_MK22F51212.c, and fsl\_clock\_MK22F51212.h are porting SoC files. Additionally, change the include path.
Change the files in board group, for example (IAR):
|
|
Ensure that board.c, board.h, clock\_config.c, and clock\_config.h are porting platform files. Additionally, change the include path.
Check the files in the sources group, for example (IAR):
|
|
The example application source files are copied when copying the example directory. Change the include path.
Change the linker file to the new platform. Ensure that the linker file is the porting SoC file.
Debug console may use UART, LPUART, or LPSCI according to the platform. As a result, the example project needs to contain UART, LPUART, or LPSCI driver files according to the platform.
|
|
For example, for TWR-K22F120M all UART files are all in the project. In another example, TWR-K80F150M, all LPUART files are in the project.
Parent topic:Porting examples
USB host CDC example
The MCUXpresso SDK debug console can be based on The MCUXpresso SDK UART, LPUART, or LPSCI driver. Because different platforms may use different drivers, the CDC has a wrapper code. The files, which call the corresponding driver API according to the debug console use UART, LPUART, or LPSCI. The utility uses the BOARD_DEBUG_UART_TYPE toidentify the UART type. To use a different UART instance, use the corresponding UART instance wrapper file.
The MCUXpresso SDK debug console only enables send. The Host CDC example needs the receive function. Therefore, configuration MACROs need to be defined in the board.h file. The debug console and the Host CDC share the same configuration. This is an example:
#define BOARD_DEBUG_UART_TYPE kSerialPort_Uart
#define BOARD_DEBUG_UART_BASEADDR (uint32_t)UART1
#define BOARD_DEBUG_UART_CLKSRC kCLOCK_CoreSysClk
#define BOARD_DEBUG_UART_BAUDRATE 115200
Update MACROs according to board design. For example, the default UART instance on the board is LPUART1, the type of default UART instance on one specific platform is LPUART, and the LPUART clock source is the external clock. In this case, change the above MACROs as follows:
#define BOARD_DEBUG_UART_TYPE **kSerialPort\_Uart**
#define BOARD_DEBUG_UART_BASEADDR (uint32_t) **LPUART1**
#define BOARD_DEBUG_UART_CLKSRC **kCLOCK\_Osc0ErClk**
#define BOARD_DEBUG_UART_BAUDRATE 115200
Parent topic:Porting examples
USB device MSC SD card example
USB device MSC SD card example needs SDHC driver support and SD card support. The example works only if the platform supports both SD card and the SDHC. To enable this example using the same code, the following MACROs are defined in the board.h file:
#define BOARD_SDHC_BASEADDR SDHC
#define BOARD_SDHC_CLKSRC kCLOCK_CoreSysClk
#define BOARD_SDHC_CD_GPIO_BASE GPIOB
#define BOARD_SDHC_CD_GPIO_PIN 20U
#define BOARD_SDHC_CD_PORT_BASE PORTB
#define BOARD_SDHC_CD_PORT_IRQ PORTB_IRQn
#define BOARD_SDHC_CD_PORT_IRQ_HANDLER PORTB_IRQHandler
Update the MACROs according to the board design. For example, the SD card detection GPIO on the board is PORTD_1. In this case, change the above MACROs as follows:
#define BOARD_SDHC_BASEADDR SDHC
#define BOARD_SDHC_CLKSRC kCLOCK_CoreSysClk
#define BOARD_SDHC_CD_GPIO_BASE **GPIOD**
#define BOARD_SDHC_CD_GPIO_PIN **1U**
#define BOARD_SDHC_CD_PORT_BASE **PORTD**
#define BOARD_SDHC_CD_PORT_IRQ **PORTD\_IRQn**
#define BOARD_SDHC_CD_PORT_IRQ_HANDLER **PORTD\_IRQHandler**
Parent topic:Porting examples
USB device audio speaker example
USB device audio speaker example needs the I2C, SAI, and DMA driver support.
The instance of SAI (I2S) and I2C are defined in the app.h file in the example directory as follows:
#define DEMO_SAI I2S0
#define DEMO_I2C I2C0
#define DEMO_SAI_CLKSRC kCLOCK_CoreSysClk
Update the MACROs according to board design. For example, the I2S instance on the board is I2S2. In this case, change the above MACROs as follows:
#define DEMO_SAI I2S2
#define DEMO_I2C I2C2
#define DEMO_SAI_CLKSRC kCLOCK_CoreSysClk
Parent topic:Porting examples
USB device CCID Smart card example
The example is based on the EMVL1 stack, which works on the EMV protocol. As a result, the example can only be ported to the platform that supports both the EMVL1 stack and the EMV protocol.
Parent topic:Porting examples
Parent topic:Porting to a new platform