Introduction

Starting with Bluetooth 4.2, Privacy can be enabled either in the Host or in the Controller:

  • Host Privacy consists of two use cases that are described in detail in the following sections. These are:

    • Random address generation - Periodically regenerating a random address (Resolvable or Non-Resolvable Private Address) inside the Host and then applying it into the Controller.

    • Random address resolution - Trying to resolve incoming RPAs using the IRKs stored in the bonded devices list. The address resolution is performed when a connection is established with a device or for the autoconnect scan. The advertising packets that have an RPA are not resolved automatically due to the high MCU processing that is required.

      The random address resolution is performed by default by the Host whenever the Controller is not able to resolve an RPA. The Host performs random address generation only when Host Privacy is requested to be enabled. During random address generation, the advertising and scan operations, if active, are stopped and restarted. If errors occur during this process and the scan or advertising cannot be started, the application is notified through the corresponding event (gAdvertisingStateChanged_c, gExtAdvertisingStateChanged_c or gScanStateChanged_c)

  • Controller Privacy, introduced by Bluetooth 4.2, consists of writing the local IRK in the Controller, together with all known peer IRKs, and letting the Controller perform hardware, fully automatic RPA generation and resolution. The Controller uses a Resolving List to store these entries. The size of the list is platform dependent and determined by gMaxResolvingListSize_c. For RPA resolution, the entries that do not fit in this list are processed by the Host to be resolved using the IRKs from Bonded Devices list.

Host Privacy can be enabled at any time. Controller Privacy should only be enabled while the device is not in the advertising, scanning or connection initiating state - otherwise the HCI LE Set Address Resolution Enable command will fail and privacy will not be considered as successfully enabled. Trying to enable one while the other is in progress generates a gBleInvalidState_c error. The same error is returned when trying to enable the same privacy type twice, or when trying to disable privacy when it is not enabled.

The recommended way of using Privacy is the Controller Privacy. However, enabling Controller Privacy requires at least a pair of local IRK and peer IRK, so this can only be enabled only after a pairing is performed with a peer and the IRKs are exchanged during the Key Distribution phase. When a device starts, if Privacy is required, the workflow is the following:

  1. Enable Host Privacy using the local IRK.

  2. Connect to a peer and perform pairing and bonding to exchange IRKs.

  3. Disable Host Privacy.

  4. Enable Controller Privacy using the local IRK and the peer IRK and peer identity address.

After enabling Host Privacy or Controller Privacy, the application must wait for the gHostPrivacyStateChanged_c or gControllerPrivacyStateChanged_c generic event and verify that privacy has been successfully enabled. Only then it is safe to proceed with setting advertising parameters (via the Gap_SetAdvertisingParameters or Gap_SetExtAdvertisingParameters APIs) or starting scanning (via the Gap_StartScanning API). Failure to do so could result in unwanted behavior, such as the device advertising or scanning with a public address.

Resolvable private addresses

A Resolvable Private Address (RPA) is a random address generated using an Identity Resolving Key (IRK). This address appears completely random to an outside observer, so a device may periodically regenerate its RPA to maintain privacy, as there is no correlation between any two different RPAs generated using the same IRK.

On the other hand, an IRK can also be used to resolve an RPA, in other words, to check if this RPA has been generated with this IRK. This process is called “resolving the identity of a device”. Whoever has the IRK of a device can always try to resolve its identity against an RPA.

For example, assume device A frequently changes its RPA using IRKA. At some point, A bonds with B. A must give B a way to recognize it in a subsequent connection when it (A) has a different address. To achieve this purpose, A distributes the IRKA during the Key Distribution phase of the pairing process. B stores the IRKA it received from A.

Later, B connects to a device X that uses RPAX. This address appears completely random, but B can try to resolve RPAX using IRKA. If the resolving operation is successful, it means that IRKA was used to generate RPAX, and since IRKA belongs to device A, it means that X is A. So B was able to recognize the identity of device X, but nobody else can do that since they do not have IRKA.

Parent topic:Introduction

Non-resolvable private addresses

A Non-Resolvable Private Address (NRPA) is a completely random address that has no generation pattern and therefore cannot be resolved by a peer.

A device that uses an NRPA that is changed frequently is impossible to track because each new address appears to belong to a new device.

Parent topic:Introduction

Multiple identity resolving keys

If a device bonds with multiple peers, all of which are using RPAs, it needs to store the IRK of each in order to be able to recognize them later (see previous section).

This means that whenever the device connects to a peer that uses an unknown RPA, it needs to try and resolve the RPA with each of the stored IRKs. If the number of IRKs is large, then this introduces a lot of computation.

Performing all these resolving operations in the Host can be costly. It is much more efficient to take advantage of hardware acceleration and enable the Controller Privacy.

Parent topic:Introduction

Parent topic:Privacy feature