HCI Black Box

This section describes the functionality, user interactions, and testing methods for the Bluetooth LE HCI Black Box demo application.

Description

The Bluetooth LE HCI Black Box demo application gives access to the Bluetooth LE Controller via a serial interface using the HCI protocol over serial interface. Refer to the Bluetooth Specification for the format of HCI commands and events over serial interface and the full list of supported commands and events.

The demo can be used with the Test Tool for Connectivity Products. The Command Console application can be downloaded from the NXP website. Alternatively you can also download it using a custom application that supports the HCI protocol and commands and events over serial interface.

Note: The HCI protocol encapsulation is dependent on the type of interface it is being used on. See the Bluetooth Specification for the HCI message format on each type of supported interface.

For instructions using the Bluetooth LE HCI Black Box with a serial terminal application or the hcitool in Linux, check the article “FRDM-KW40Z Bluetooth LE Controller Usage with the Linux hcitool”.

Parent topic:HCI Black Box

Supported platforms

The following platforms support the HCI Black Box application:

  • KW45B41Z-EVK

  • FRDM-MCXW71

  • MCX-W71-EVK

  • KW47-EVK

  • FRDM-MCXW72

  • MCX-W72-EVK

Parent topic:HCI Black Box

Usage with Test Tool for Connectivity products

The Bluetooth LE HCI Black Box demo application is designed to be used via serial interface. This can be achieved using the TEST Tool for Connectivity Products – Command Console application as described below.

  1. Download the demo application to a supported board.

  2. Connect the board to a USB port of the PC. The UASB COM port drivers must be installed properly and a COM port corresponding to the board should be available.

  3. Open the Test Tool application and connect to the serial port corresponding to the board on which the Bluetooth LE HCI Black Box application runs. The serial communication parameters are: baud rate 115200, 8N1, and no flow control. See the figure Test tool command console serial port selection below.

    Test tool command console serial port selection

  4. Select the appropriate Test Tool HCI XML file from the drop-down list for the release you are using. Send a few commands to the application. An example is shown in the figure HCI black box command example below.

    HCI black box command example

Parent topic:HCI Black Box

Parent topic:Bluetooth LE stack and demo applications