APS codes
The APS codes relate to sending/receiving messages.
APS codes
Name |
Value |
Description |
---|---|---|
ZPS_APL_APS_E_ASDU_TOO_LONG |
0xA0 |
A transmit request failed since the ASDU is too large and fragmentation is not supported. |
ZPS_APL_APS_E_DEFRAG_DEFERRED |
0xA1 |
A received fragmented frame could not be defragmented at the current time. |
ZPS_APL_APS_E_DEFRAG_UNSUPPORTED |
0xA2 |
A received fragmented frame could not be defragmented since the device does not support fragmentation. |
ZPS_APL_APS_E_ILLEGAL_REQUEST |
0xA3 |
A parameter value was out of range. |
ZPS_APL_APS_E_INVALID_BINDING |
0xA4 |
An APSME-UNBIND.request failed due to the requested binding link not existing in the binding table. |
ZPS_APL_APS_E_INVALID_GROUP |
0xA5 |
An APSME-REMOVE-GROUP.request has been issued with a group identifier that does not appear in the group table. |
ZPS_APL_APS_E_INVALID_PARAMETER |
0xA6 |
A parameter value was invalid or out of range. |
ZPS_APL_APS_E_NO_ACK |
0xA7 |
An APSDE-DATA.request requesting acknowledged transmission failed due to no acknowledgment being received. |
ZPS_APL_APS_E_NO_BOUND_DEVICE |
0xA8 |
An APSDE-DATA.request with a destination addressing mode set to 0x00 failed due to there being no devices bound to this device. |
ZPS_APL_APS_E_NO_SHORT_ADDRESS |
0xA9 |
An APSDE-DATA.request with a destination addressing mode set to 0x03 failed due to no corresponding short address found in the address map table. |
ZPS_APL_APS_E_NOT_SUPPORTED |
0xAA |
An APSDE-DATA.request with a destination addressing mode set to 0x00 failed due to a binding table not being supported on the device. |
ZPS_APL_APS_E_SECURED_LINK_KEY |
0xAB |
An ASDU was received that was secured using a link key. |
ZPS_APL_APS_E_SECURED_NWK_KEY |
0xAC |
An ASDU was received that was secured using a network key. |
ZPS_APL_APS_E_SECURITY_FAIL |
0xAD |
An APSDE-DATA.request requesting security has resulted in an error during the corresponding security processing. |
ZPS_APL_APS_E_TABLE_FULL |
0xAE |
An APSME-BIND.request or APSME.ADDGROUP.request issued when the binding or group tables, respectively, were full. |
ZPS_APL_APS_E_UNSECURED |
0xAF |
An ASDU was received without any security. |
ZPS_APL_APS_E_UNSUPPORTED_ATTRIBUTE |
0xB0 |
An APSME-GET.request or APSMESET. request has been issued with an unknown attribute identifier. |
Parent topic:Return/Status Codes