Discovery
The ZigBee specification provides the facility for devices to find out about the capabilities of other nodes on a network, such as their addresses, which types of applications are running on them, their power source and sleep behavior. This information is stored in descriptors (see Section 3.4.6) on each node, and is used by the enquiring node to adapt its behavior to the requirements of the network.
Discovery is typically used when a node is being introduced into a user-configured network, such as a domestic security or lighting control system. It may require the user to press a button or similar to begin the process of integration of the device into the network. The first task is to find out if there are any appropriate devices with which the new node can communicate.
Device discovery
Device discovery returns information about the addresses of a network node. The retrieved information can be the IEEE/MAC address of the node with a given network address, or the network address of a node with a given IEEE/MAC address. If the node being interrogated is a Router or Coordinator, it may optionally supply the addresses of all the devices that are associated with it, as well as its own address. In this way, it is possible to discover all the devices on a network by requesting this information from the Coordinator (network address 0x0000) and then using the list of addresses corresponding to the children of the Coordinator to launch other queries about their child nodes.
Parent topic:Discovery
Service discovery
Service discovery allows a node to request information from a remote node about the remote node’s capabilities. This information is stored in a number of descriptors (see Section 3.4.2) on the remote node. It includes the following:
The device type and capabilities of the node.
The power characteristics of the node.
Information about each application running on the node.
Optional information such as serial numbers.
Other user-defined information - for example, easily understandable names such as ‘MtgRoomLight’.
Requests for these descriptors are made by a device during the discovery process that is typically part of the device’s configuration and integration into a ZigBee network.
Parent topic:Discovery
Parent topic:Application level concepts