End device aging
A Router that is a parent needs to maintain its Neighbor table. This involves discarding inactive children (that may have left the network) in order to make way for potential new children. An End Device Aging mechanism is available to support this maintenance.
In this mechanism, a timeout is applied to every child entry in the Router’s Neighbor table. If a packet, called a ‘keep-alive’ packet, is not received from an End Device child before its timeout expires, the child is assumed to be no longer active and is removed from the table (and therefore from the Router’s children).
Timeout period
The timeout period is specific to an individual child and is set on the End Device using the function zps_bAplAfSetEndDeviceTimeout(). This period is communicated to the parent via an End Device Timeout Request when the End Device joins (or re-joins) the network. The timeout is applied by the Router to the Neighbor table entry for the End Device. The arrival of a keep-alive packet from the End Device will result in the timeout being re-started from the beginning. If the timeout is allowed to expire (without a keep-alive packet), the Router will delete the relevant child entry from the Neighbor table.
Note 1: The Router initially sets the timeout for all End Device children to the default value defined in the NIB, which is 256 minutes in the NXP software. The timeout will remain at this value unless changed by the End Device, as described above.
Note 2: After receiving the End Device Timeout Request, the parent will send an End Device Timeout Response to the End Device, indicating the outcome of the request. If the request has been successful, the End Device can subsequently send keep-alive packets
Parent topic:End device aging
Keep-alive packets
A keep-alive packet can be sent from the End Device using the function zps_eAplAfSendKeepAlive(). It is recommended that this function is called at least three times within the timeout period defined for the End Device, in order to prevent the child from being accidentally removed from the network due to missed keep-alive packets at the parent.
A keep-alive packet can be either of the following types:
MAC Data Poll: In this case, the parent may send pending data back to the End Device. The arrival of this data at the End Device will be indicated by a zps_EVENT_AF_DATA_INDICATION event (as described in Section 6.5.2).
End Device Timeout Request: This packet type simply has the effect of re- starting the timeout for the End Device on the parent, which will return an End Device Timeout Response to the End Device, indicating the outcome of the request.
The keep-alive packet type to be used is determined by the Router parent and is configured in the NIB on the parent - in the NXP software, a Router is configured to accept either packet type, by default. This information is communicated to the End Device in the initial End Device Timeout Response that is sent to the End Device on joining the network. The zps_eAplAfSendKeepAlive() function will then automatically send the appropriate keep-alive packet type - where either packet type is accepted by the parent, the function sends a Data Poll packet.
Parent topic:End device aging
Parent topic:Advanced features