Finding compatible endpoints
An endpoint on a newly joined node must find compatible endpoints on remote nodes with which to communicate. The decision of whether a remote endpoint is compatible is based on the endpoint properties stored in its Simple descriptor, notably the input/ output clusters supported.
The endpoint application can discover compatible nodes by sending out a Match_Desc_req request identifying the required clusters. This request is submitted by calling the function zps_eAplZdpMatchDescRequest(), which allows the request to be sent as a broadcast to all nodes or as a unicast to a particular node (the sending node may already have a record of the network nodes and their addresses, as each node automatically announces itself in a broadcast when it joins the network). The
request is sent in an APDU (Application Protocol Data Unit) which must first be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance().
A receiving endpoint which satisfies the supplied criteria replies to the request with a Match_Desc_rsp response which, when received, must be collected on the requesting node using the function ZQ_bZQueueReceive(). The requesting application may bind to a compatible endpoint (see Section 5.4) and communicate with the endpoint using binding or addressing (see Section 5.5).
Parent topic:Discovering the network