Appendix C: Implementation of frame counters
Frame counters are used to prevent message replay attacks (see Section 2.10, “Secure operating environment”). Each message sent across the network carries a frame count. It is inserted by the sending node and is part of a sequence of frame counter values for messages from this node.
Two types of frame counter exist:
NWK frame counters: These are implemented automatically at the NWK layer of the stack and are used in all network communications.
APS frame counters: These are optional and applied by the APS layer of the stack to one or more specific source/destination links.
The rest of this section describes the standard NWK frame counters. Detailed information on NWK and APS frame counters can be found in the ZigBee 3.0 specification.
A node locally maintains two types of NWK frame counters:
Outgoing frame counter: A single frame counter for all sent messages is maintained in RAM. It is incremented every time a message is transmitted (to any destination node) and its value is inserted in the message. Its value can be persisted in non-volatile memory - the NXP method of persisting this counter is described later.
Incoming frame counters: A frame counter is maintained in RAM for every node in the local Neighbor table. It records the frame count contained in the last message received from this node. Persisting the frame counters for all neighbors would use too much space in non-volatile memory. Hence, its value is not persisted. On a power-cycle or reset, these values are all reset to 0.
If a destination node receives a message containing a frame count which is less than the locally held incoming frame counter value for the same source node (corresponding to the frame count of the previous message received from the source node), it rejects the message. The receiving node informs the rest of the network by sending out a Network Status command with a status value of 0x11 (bad frame counter).
A problem might occur if the outgoing frame counter is not persisted and reverts to 0 when the node is reset. This would result in messages being sent with a frame count lower than the value expected by the destination node(s). Consequently, the messages from this node would be rejected.
Persisting the outgoing frame counter is therefore advisable, but doing this on every update of the counter causes excessive Flash wear. To minimize this wear, the NXP stack software only persists the outgoing frame counter every time it reaches a multiple of 1024. If the node is reset, the current frame counter value is likely to be greater than the persisted value, so 1024 is added to the recovered value. This ensures that the outgoing frame counter is always larger than the value in the last message sent before the reset.
For example, consider a case when the last message transmitted had a frame count of 4000 and then the node is reset. In such a case, the last persisted value of 3072 is recovered but 1024 is added to it to make an outgoing frame counter of 4096 (which will be persisted).