Received message queues
All messages received ZPS_msgMcpsInd on a network node are pushed into one of the following two queues:
ZPS_msgMcpsDcfm
ZPS_msgMcpsInd
These queues must be created by the application using the function ZQ_vZQueueCreate(). An example code is described in Section 6.9.1.2.
ZPS_msgMcpsDcfm
All IEEE 802.15.4 MAC data deferred confirm events are added to this queue. The default size of this queue is 8 but a different queue size can be set when the queue is created. The queue can overflow if there is heavy network traffic.
Parent topic:Received message queues
ZPS_msgMcpsInd
All IEEE 802.15.4 MAC data packets are added to this queue. The default size of this queue is 24 but a different queue size can be set when the queue is created. The queue can overflow if there is heavy network traffic.
Parent topic:Received message queues
Parent topic:Appendix B: Application design notes