Simple descriptor
The Simple descriptor for an application includes:
The endpoint on which the application runs and communicates
The ZigBee device type that the application implements
The ZigBee clusters that the device type implements
Whether there are corresponding Complex and User descriptors
Lists of input and output clusters (see Section 3.4.1) that the application uses and provides, respectively
Parent topic:Descriptors