tszQueue
The ZigBee queue structure tszQueue
is shown below.
typedef struct
{
uint32 u32Length;
uint32 u32ItemSize;
uint32 u32MessageWaiting;
void *pvHead;
void *pvWriteTo;
void *pvReadFrom;
}tszQueue;
where:
u32Length
is the size of the queue in terms of the number of messages that it can holdu32ItemSize
is the size of a message, in bytesu32MessageWaiting
is the number of messages currently in the queuepvHead
is a pointer to the beginning of the queue storage areapvWriteTo
is a pointer to the next free place in the storage area where a new message can be writtenpvReadFrom
is a pointer to the next message to be read from the storage area
Parent topic:ZigBee queue structures