ZDP codes

The ZDP codes are carried in request and response messages.

ZDP codes

Name

Value

Description

ZPS_APL_ZDP_E_INV_REQUESTTYPE

0x80

The supplied request type was invalid.

ZPS_APL_ZDP_E_DEVICE_NOT_FOUND

0x81

The requested device did not exist on a device following a child descriptor request to a parent.

ZPS_APL_ZDP_E_INVALID_EP

0x82

The supplied endpoint was equal to 0x00 or between 0xF1 and 0xFF.

ZPS_APL_ZDP_E_NOT_ACTIVE

0x83

The requested endpoint is not described by a Simple descriptor.

ZPS_APL_ZDP_E_NOT_SUPPORTED

0x84

The requested optional feature is not supported on the target device.

ZPS_APL_ZDP_E_TIMEOUT

0x85

A timeout has occurred with the requested operation.

ZPS_APL_ZDP_E_NO_MATCH

0x86

The End Device bind request was unsuccessful due to a failure to match any suitable clusters.

ZPS_APL_ZDP_E_NO_ENTRY

0x88

The unbind request was unsuccessful due to the Co- ordinator or source device not having an entry in its binding table to unbind.

ZPS_APL_ZDP_E_NO_DESCRIPTOR

0x89

A child descriptor was not available following a discovery request to a parent.

ZPS_APL_ZDP_E_INSUFFICIENT_SPACE

0x8A

The device does not have storage space to support the requested operation.

ZPS_APL_ZDP_E_NOT_PERMITTED

0x8B

The device is not in the proper state to support the requested operation.

ZPS_APL_ZDP_E_TABLE_FULL

0x8C

The device does not have table space to support the operation.

ZPS_APL_ZDP_E_NOT_AUTHORIZED

0x8D

The permissions configuration table on the target indicates that the request is not authorized from this device.

Parent topic:Return/Status Codes