Zigbee application support resources

While developing your ZigBee 3.0 application for a JN518x or K32W041/K32W061/K32W1/MCXW71/MCXW72/RW612 device, refer to the below User Guides along with JNUG3130:

  • ZigBee Devices User Guide (JNUG3131)

  • ZigBee Cluster Library User Guide (JNUG3132)

  • Connectivity Framework Reference Manual

Refer to the following NXP Application Notes for further support in the development of ZigBee 3.0 applications for the JN518x or K32W041/K32W061/K32W1/MCXW71/MCXW72 devices:

  • ZigBee 3.0 Base Device Template (JN-AN-1217)

  • ZigBee 3.0 Light Bulbs (JN-AN-1244)

  • ZigBee 3.0 Controller and Switch (JN-AN-1245)

  • ZigBee 3.0 Sensors (JN-AN-1246)

  • ZigBee 3.0 IoT Control Bridge (JN-AN-1247)

For RW612 devices, refer to ZigBee 3.0 Light Bulbs**JN-AN-1244 .

Note: The relevant software and documentation resources can be obtained via the Wireless Connectivity area of the NXP website (for the web address, see Support resources.

Parent topic:Application development overview