ZPS_eAplAibRemoveBindTableEntryForMacAddress

ZPS_teStatus
    ZPS_eAplAibRemoveBindTableEntryForMacAddress(
                            uint64 u64MacAddress);

Description

This function requests the removal of the entry corresponding to the specified IEEE/ MAC address from the local binding table.

Parent topic:ZPS_eAplAibRemoveBindTableEntryForMacAddress

Parameters

u64MacAddress IEEE/MAC address contained in the binding table entry to be removed

Parent topic:ZPS_eAplAibRemoveBindTableEntryForMacAddress

Returns

ZPS_E_SUCCESS

Parent topic:ZPS_eAplAibRemoveBindTableEntryForMacAddress

Parent topic:Binding functions