ZPS_psNwkNibGetHandle
ZPS_tsNwkNib *ZPS_psNwkNibGetHandle(void *pvNwk);
Description
This function obtains a handle for the NIB (Network Information Base) corresponding to the specified NWK layer instance.
The function should be called after ZPS_pvAplZdoGetNwkHandle(), which is used to obtain a pointer to the NWK layer instance.
The NIB is detailed in the ZigBee Specification (05347) from the ZigBee Alliance. This function is not strictly a ZDO function.
Parent topic:ZPS_psNwkNibGetHandle
Parameters
pvNwk Pointer to NWK layer instance
Parent topic:ZPS_psNwkNibGetHandle
Returns
Pointer to NIB structure
Parent topic:ZPS_psNwkNibGetHandle
Example
void *pvNwk; = ZPS_pvAplZdoGetNwkHandle();
ZPS_tsNwkNib *pNib = ZPS_psNwkNibGetHandle(pvNwk);
Parent topic:ZPS_psNwkNibGetHandle
Parent topic:Object Handle functions