ZPS_tsAfBindRequestServerEvent

This structure is used in the ZPS_EVENT_BIND_REQUEST_SERVER event, which reports the status of a data transmission sent from the (local) node to a set of bound endpoints.

The ZPS_tsAfBindRequestServerEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint8 u8SrcEndpoint;
    uint32 u32FailureCount;
} ZPS_tsAfBindRequestServerEvent;

where:

  • u8Statusis the overall status of the bound data transmission:

    • Success (0) indicates that the data packet was successfully transmitted to all bound endpoints

    • Failure (non-zero value) indicates that the data packet was not successfully sent to at least one bound endpoint (see u32FailureCountbelow).

  • u8SrcEndpointis the number of the local endpoint from which the data packet was sent.

  • u32FailureCountis the number of bound endpoints for which the transmission failed.

Parent topic:Event structures